This tool is reserved for Profibus"Process Field Bus" Profibus is the most popular type of fieldbus (see Fieldbus entry in the glossary) used worldwide fieldbusesA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design only.
To open the I/O Editor select Tools>Custom IO Editor from the menubar.
Figure 10-39: Input/Output Editor
For the Description field, see format explanations.
|
Copyright © 2015 Kollmorgen™ |
|